Kontak
PT. igus® Indonesia

Taman Tekno BSD

Sektor XI, Blok L1 No. 15

Tangerang Selatan 15314

+62 21 7588 1933
+62 21 7588 1932

Chemist prescription printer

Precise and effective

This prescription printer, which is used in pharmacies, fits into the limited space of a cash desk drawer. The printer is one of the most important components of the cash desk, as failure prevents prescriptions from being processed and thus means a sales shortfall. Absolute accuracy is also required for a precise typeface. The ink cartridge holder slides on the metal guide rod with two iglidur® J plain bearings, whilst two additional guides on the metal lip help it to run parallel. The guide rod was assembled with igus® MCM clip bearings.

Thorbjörn Missalek, JDM Innovation GmbH, Murr
 
 
More on applied products here
Further interesting applications from extremely diverse areas can be found here.
Go to manus® contest